AXIS#.IL.KPDRATIO

Description

This parameter reads the proportional gain of the PI-loop which controls the d-component of the current.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 100

Default Value

1

Data Type

Float

See Also

AXIS#.IL.KP

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.KPDRATIO

500ah

03h

Unsigned32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5872

1

5872 (0x16f0)

AXIS1.IL.KPDRATIO

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.KPDRATIO

5872

Float

Read Only

-